Dear Sir/Ms.
My client wants to use the TPS92663 to complete the Fade in and Fade out functions. His expectation is to set a final brightness (perhaps 90%) and a lighted time slope and then the set up a flag or an instruction. The TPS92663 can be brightened slowly. Set a final brightness (perhaps 5%) followed by a darkened time slope and then the next instruction. TPS92663 can slowly dim. But we can't find this function in the datasheet. Does the TPS92663 have such a function?
Best Regards,
Kami Huang