Hi,
Is it possible to force the max current 3.1A on PMID pin if i don't use the USB interface but just by I2C or by a pin configuration?
Best Regards,
Serge.
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Serge,
The voltage at VBUS will be seen at PMID but there is no current limiting by the RBFET itself. The RBFET only measures current. Any current pulled from PMID will not be available to provide a power to SYS and/or the battery at BAT. PMID has no short circuit protection so if pull too much current (>5A) you could damage the RBFET.