This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

BQ25505: setting of MPPT

Part Number: BQ25505


Hi teams,

When setting 80% of MPPT, is it possible by connecting VSTOR to VOC_SAMP?
Also, is it possible to set it to 80% or more?

When actually testing with EVM, it became about 75% when VSTOR was connected to VOC_SAMP, is it within the allowable range?

Best regards,

Hayashi