Part Number: BQ24161
Other Parts Discussed in Thread: BQ25600, BQ25601
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Part Number: BQ24161
Other Parts Discussed in Thread: BQ25600, BQ25601
Hi team,
Not sure if the images in the first posted attached so want to include them here again.
Thanks and best,
Jerry
Hi Jerry,
Since ideal charge level for battery is 80%, I would also like to check if this termination current issue can be bypassed if we were to charge the battery using 80% (3.7V) of voltage level. Base on your team's experience, how does your customers charge their battery if they didn't want a full charge for battery longevity reasons?
Thanks,
Yu Yin
Is there a recommended battery for this charger that is high in capacity/Ah?
Would setting the volt(reg) to be at 3.7V(80%) instead of full capacity bypass this termination current issue?
If not, then a charge that allows: