This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

TPS65910: Silicon version

Guru 16770 points
Part Number: TPS65910

Hi

What is the latest silicon version of TPS65910?

Could it be possible that the silicon version is other than ES1.1 with the design from now on?

BestRegards

  • I have forwarded your question to the product specialist for this part.
  • na na78,

    Silicon Errata ES1.1 is not the silicon version #. The ES1.1 is just a short numbering system for errata counting, but there is only one errata for this device. If another Errata were released, it would be called ES1.2

    The silicon version number is contained in Register 0x80 as seen on page 94 of the datasheet, VERNUM[3:0]

    You can read this register to determine the silicon version of the device.

    It is my understanding that all released silicon ends with the digits "-A1" before the package code (RSL) and the full Reel letter (-R).

    For example, the TPS65910A1RSL means it is the basic TPS65910 variant, it is -A1 silicon version, and RSL is the package.

    The ES1.1 Errata applies to all silicon in the TPS65910 Product Folder, which is the -A1 silicon version, and no other silicon versions are available on the web.