When evaluate the TPS546116, I got 3 questions and need help please:
1. The input voltage in datasheet is 3V-6V, but the output voltage for this chips is 3.3v. The low limit of the input voltage (3V) seems not right, what is the lowest voltage should I give if I want to get a 3.3V output?
2. The IQ current I measured is about several mA larger than the datasheet (fs=350kHz, low limit is 9.6 mA and fs=550kHz is 12.8mA), is this right?
3. The enable voltage of SS/ENA pin in datasheet is 1.2V, but the chip can start when I give near 3V voltage, is the 1.2V on datasheet a wrong value?
Thanks.