This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

TPS7B6350EVM: Thermal Data

Part Number: TPS7B6350EVM

Dera, Sir.

My customer is foocusing Infineon/TLS850F1TA V50 for their system,

Vin_max=16V, Vin_typ=12V, Io=250mA.

The product is D2PAK to consider the better thehrmal performamnce.

Against it, I am considering to promote TPS7B6350-Q1, HTSSOP16.

Is it possible to show the thermal data of TPS7B6350EVM if you have?

The package top temperature & ambient temperature would be good reference

for us.

I am hoping to get your advice.

Best Regards,

H. Sakai

  • Hi H. Sakai,

    We provide the thermal metrics of our devices within the datasheet in the Thermal Information table.  Since application specific layout can significantly impact thermal performance, we model ICs following a standardized process as specified by the JEDEC in the EIA/JESD51-x series of documents.  While this data is modeled on a JEDEC High-k board, it is important to note that our team updates the model to ensure a strong correlation to real board measurements.

    Very Respectfully,

    Ryan