Other Parts Discussed in Thread: EV2400, BQSTUDIO, BQ25882
Dear TI,
I was wondering if the bq25881 can be used as a standalone device?
For example, once the configurations are all set up with bqStudio and the EV2400, will it operate as a powerpath management system accepting a charge and providing power to the system?
Also, if power to system is provided by the battery only (2S configuration) can it output 5V up to 2A?
I imagine this could be set up with bqStudio.
If the answers are yes to the above questions, this is a perfect new solution for several applications!
Thanks much,
Kevin