Hi
Please would you be able to assist me with the following?
1. Do you have a more detailed datasheet for the TPS2HB16-Q1 device? The one available from TI is only a 10 page document which does not have many of the parameters and curves that I am looking for.
2. If a more detailed datasheet is not available, then will it be possible to at least know :
(i) the over current protection limit of the device
(ii) the maximum safe continuous current that could be drawn from the device (with the case held at 85 deg celcius
Thank you,
Lakshman