This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

TPS74701: Debugging issues.

Part Number: TPS74701


We have seen several failures on a small number of boards.  When they fail the FB pin is aprox  0.6V instead of the 0.8V so the output is always low.

Is there any errata on these parts?  It seems to vary with date code. One date code we saw had no errors. TPS74701DRCR

Thanks

Dan

 

  • Hi Dan,

    We do not have any errata on TPS74701. Any errata would be published to the product folder.

    So that I can better understand your how the rails are interacting in your application, can you provide a multi-channel scopeshot with Vin, Vout, Ven, and Vbias? Also if you change the load current, do you see a difference in the output voltage?

    Very Respectfully,
    Ryan
  • Hi Dan,

    Since it has been several weeks without a reply, I assume that this thread is resolved. If this is not correct, please feel free to post again.

    Very Respectfully,
    Ryan