Hello,
We are attempting to synchronize two UCC2897A so that they operate out of phase.
The datasheet states that if you directly connect the SYNC pin from one UCC2897A to another, then they will operate in phase.
A simple solution seems to simply delay the pulse so that the received pulse is 180 degrees output of phase with the original pulse.
- Page 14 of the datasheet says any synchronizing frequency applied to the SYNC pin must be greater than the internal oscillator. However, Page 14 also says when SYNC is outputting pulses they are driven from the internal oscillator. How can one UCC2897A send synchronizing pulses to another UCC2897A if the pulses cannot satisfy the 'greater than the oscillator frequency' requirement?
- Page 14 states that the SYNC pin is bi-directional. How is the SYNC pin configured as an input or an output? How do we keep two UCC2897A from clashing with each other if they both are trying to send pulses on SYNC?
Thank you,
Ryan B.