I am design a DC - DC 3V-4V / 2A (Li-ion battery cell 0.2C discharge current) to 14V 250mA convertor to charge 12V Pb battery , working with a TPS61085. I follow the design document to connect the wire and check every connection is correct then power on it with no load condition. But unfortunaltly, it doesn't work. I measure all the pin reading with FLUKE multi meter, Pin 2 (FB) alwayse a 4.85V out (Pin 6 Vcc = 5V) . At no output condition, it should be 0V. Original design is 156K serial 18K between Vout and Ground. Center pin of two resistor connect to Pin 2(FB). I try to connect 1K ohm to ground, still the same as 4.85V. Even I short Pn 2 to Ground, TPS61085 work just once at the spot when touch ground.
Then I try to switch this FB pin to ground on and off quickly, output pin seems get 14V voltage but suddently it burn out.
Can some on tell me where I might be wrong? Or similar experience?
I bought 4 units from DIGI-key last week. Feel sad at this test result.
Thanks
Tommy