Hi,
The sever in the picture is PSE, connect to the midspan(UPoE injector) then connect to PTZ.
The detection mechanism of different vendor's PSE are also different. Some of them are keeping dectect and class..., but some of them detect of only if RJ-45 plug-in.
When using PSE(detect only when RJ-45 plug-in)+ UPoE injector, the power sourcing work well.
When using PSE(keeping detect type)+ UPoE injector, the power sourcing doesn't worked sometimes(result form the PSE's sequence or voltage can't meet injector's, then PoE start-up sequence error)
And this is what our end-customer found, when use sever with PSE + UPoE injector, the PTZ can't get power after power plug-in. After analysis, we found the hot-swap MOS is shorted to GND.
So we suspect that the inrush current of PSE and injector makes internal MOS(hotswap mos) damaged. The fail rate is 0.01%.
Here are the question:
1.May I know is there any issue happened like this before?
2.Or any way to prevent this?