In one of your data sheets (SLVS044X –SEPTEMBER 1997 –REVISED SEPTEMBER 2016) referring to the LM317 precision voltage regulator, section 8.3.4 (figure 15) on page 12, A Tracking Preregulator Circuit is shown.
I know the LM313 is an ageing technology, but it works and it's cheap!
There is a 5v difference or 'headroom' from the output of the first regulator to the second (as I understand).
Now for a single regulator the maximum supply voltage is 40v, so does this mean for two LM317s in this configuration 'raw DC' supply can be increased to say 45v, or higher?
I'd like to build a variable regulator 0-30v but I get the feeling i could be approaching 40v maximum, which is the upper limit of just a single LM317, but I feel two LM317s in series (as per figure 15) could be supplied with greater headroom and a higher 'raw DC' supply.
Thanks for any help you may be able to provide,
Trevor Brearley