This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

BQ27220: Current measurement capacity

Part Number: BQ27220

Hello!

I'm trying to find the current measurement capacity of BQ27220. I believe its calculated as follows:
Imeasured=(Vsrn-Vsrp)/Rsense

From the datasheet, following are the values which are gathered: (Vsrn-Vsrp)=2V; Rsense=10mohm. Does this mean that the maximum current measurement capacity is 200 A? Please indicate any mistakes with my understanding of current measurement.

Also, what is the max. charge discharge current for BQ27220EVM-744? Some EVM datasheets list these limits, but I couldn't find that in the datasheet of this product.

Thanks!