I would like to have VVOD.1 on the EV2400 to be enabled so as to power my BMS.
It is marked "Optional voltage output (future expansion)" and the enable pin for this is connected to P7.4 (pin 57) of the MSP430 controller. It is possible to do this out of the box now? Otherwise I need to solder a cable to bring power to VOUT1 from somewhere else.
The output I want enabled VVOD.1:
The source of it:
The pin that enables it:
Can somebody advise?