This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

Recommend a power IC used to the image sensor

Other Parts Discussed in Thread: TLV707P, LP5907, LP5912

Dear Engineers,

Can you recommend a power IC for me?

The power module meets the following characteristics:

  1. Used to power the image sensor;
  2. The common mode rejection ratio parameter is better;
  3. Low noise;
  4. High cost performance;
  5. The input voltage is 5.5V/6V, and the output voltage is adjustable from 1.5V to 3.3V.

Thank you very much!

BRs!

Elsa Duan

  • Hi Elsa,

    Thanks for sending this request over and  providing this information! What image sensor are you going to be powering? I am interested in the output current that is going to be used.

    For now, I can recommend some of our hero devices for image sensors. Please check out: LP5907, LP5912 and TLV707P

    Thanks,

    Wilson