Other Parts Discussed in Thread: LM25119, LM5143-Q1, LM5140-Q1
Hi TI,
Kindly suggest me the best suitable dc-dc converter.
Requirement
Input: 12V
Output: 11V/ 50Amax
I couldn't find suitable converter.
So, Can I use TPS40170 in parallel? I'm wondering about OCP, SCP.
And maximum output current of LM25119 is 40A, If I use with external gate driver, Can it be up to 50A?