Other Parts Discussed in Thread: BQ25640,
Hi,
I am a little bit confused with the parameter charge current, which is calculated according to the given formula in the datasheet. I would like to use this IC for charging 2 supercapacitors (45F/5.6V) rated from Visay. I have a +10V supply delivering 3A max. limit as input to my circuit. Since I would somehow use some two schottkey diodes in series for reverse protection. The supply votlage is a little bit down to 9.6-9.7V.
From the datasheet of the supercaps 196 HVC ENYCAP in Table 3 (Part. Nr: MAL219690202E3) it says, the recommeded charge current is 30-300mA and 0.5A is the maximum for both charge and discharge.
Does that mean that I have to set the charge current setting to only 0.5A max. for this supercapacitor stack. I want to charge the supercaps each to 4.8V (9.6V). which means I have almost equal to 0.98 duty cycle from my half bridge configuration.
Thank you.