Hi,
I am trying to charge a battery with 3 cells that has a max value ~ 4.8V with a current of 1A.
When I visualize the power supply I see that all is well (the current injected to the bq25703a is ~ 1A) but when I consulted the registers: ChargerStatus (21 / 20h) and ADCIBAT (29 / 28h) I noticed that the current is set at 384 mA and the charger is in pre-charge.
How can I configure the BQ25703a to work in fast mode with a current of 1A?
Regards,