This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

WEBENCH® Tools/LM22678: LM22678: LM22678TJ-5.0/NOPB Mejor component selection inductor selection query?

Part Number: LM22678

Tool/software: WEBENCH® Design Tools

Hello All
Greetings!!!!!!
We have designed switcher using LM22678TJ-5 for 5A.
Input Maximum voltage: - 30V DC using the battery pack
Please see attached schematic design photo.

We need a suggestion for my major component selection right or not, please find below component specification.

Inductor Part Number:- Mfr. No: 744325650\6.5UH 8.4A 12.5 MOHM OR SRR1208-6R5ML\6A 18 MOHM

Please suggest which inductor part will be use full for our switcher We need to require 5V/5A constant output.
Thank you in advance

Hardik Jani