Other Parts Discussed in Thread: BQ25703
Hello,
i am wondering, which Ground to use for the capacitor at the VDDA Pin on a BQ25703.
The Datasheet says under 6 Pin Functions to use PGND and shows in 9.1 Typical Application GND. In The EVM bq2570x it is also tied to GND.
I surmise, that the VDDA voltage is also used for meassurement of the input current over the shunt and so it would be better to tie it to PGND.
Best Regards and Thanks