Part Number: BQ76920
Tool/software: Code Composer Studio
Hello,I have two problems. Please help me out:
Question 1:I have four batteries, so the actual 4 and 5 legs of the con6 are short.Is the equalization that the chip will automatically detect the pressure difference between the battery pack to make the action?Or do I need my software to detect the voltage of 4 sets of batteries, and then write the corresponding value to register CELLBAL1 in real time to control the battery discharge according to the battery pressure difference?
Question 2:Data sheet indicate that adjacent batteries cannot be balanced at the same time, but CB0:VC0~VC1, CB1:VC1~VC2, CB2:VC2~VC3, CB3:VC3~VC4, CB4:VC4~VC5(short connection), CB5:VC5~VC6,
So if I set CB4 to 0 all the time, then things like CB0 and CB1 can't be balanced at the same time, what about CB3 and CB5?Is it adjacent?
Attached schematic