This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

TPS92662-Q1: Technical documents and detailed specifications about TPS92662-Q1

Part Number: TPS92662-Q1

Want to know the difference between 92662 and 92661?

And output current needs 1A, I don't know if 92661 can be used up to 100%
Would that 92626 be better?

How to get technical documents and detailed specifications about TPS92662-Q1?

  • Hello Alan,

    Both TPS92661 and TPS92662 are good for 1A at 100%

    Some differences:

    The TPS92661 is capable of 2.0 A per switch continuous.

    The 661 uses 5V for Vin where the 662 uses up to 60V.

    The 661 has the capability to do 3.3V or 5.0V I/O.
    The 662 has the capability to do 3.3V or 5.0V I/O.

    To get more information it needs to be requested through the TI website:
    Example, search TPS92662, click on the part to get to the datasheet and you will see a request window.

    Best Regards,