Part Number: LM3402
Other Parts Discussed in Thread: TPS92640
Hi Team,
My customer is looking for solution for adjustable current source, below is the requirements:
Channel: 2
Adjustable Current: 0A~2A
Maximum load: 25ohm
Ripple: Vrms<=10mV, Vpp<=100mV
Response time <=100ms
Accuracy: +/-2%
Would you pls help check if we have solution to meet above requirements? Thanks.
Best regards,
Sulyn