Other Parts Discussed in Thread: , TPS65217, TPS65218D0
My goal is to have DCDC1 turn off, once the battery has finished charging from AC (the AC will remain connected).
But I can't get DCDC1 to turn off if AC is live. Setup is like so:
PB_IN pin remains pulled up to VSYS at all times.
I set DEFDCDC1.B7=0 (which allows control via the pin), then drive pin HOLD_DCDC1 low.
This should turn off the DCDC1. And it does turn off when AC is dead. But it does NOT turn off when AC is live.
Anyone have any ideas?