Other Parts Discussed in Thread: BQ20Z45, BQ40Z50
Hello,
If FETs are off and are in shutdown mode, what would the output measure from Pack + to Pack - ?
Thanks,
Mike
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Hello,
If FETs are off and are in shutdown mode, what would the output measure from Pack + to Pack - ?
Thanks,
Mike
Batt,
I apologize, I may have been confusing. There is no charger attached at all, so we are talking about the open circuit voltage on the output of the pack after it shuts off. Pack - stays at the same level as Batt -, as it is not broken and only has the sense resistor between them. Pack + is separated from Batt + by the FETs, so in shutdown mode, what is the voltage I should expect to measure across Pack + and Pack -?
Thanks,
Mike
Batt,
I don't know if that is true, and in fact have never seen that. I've typically seen around 0.5 - 0.8V when the FETs are OFF. In my mind, I will read whatever the pack + side floats to in reference to pack -. I know for my circuitry that when Pack+ is disconnected from Batt+, I don't have a single resistor that would pull that net down to GND to give me 0V. Therefore, I'm basically asking what is internal to your part that would pull this net down where you think I should have 0V across Pack+ and Pack- during shutdown?
I'm not concerned about anything, even if I had 1V on the output during shutdown, the second any sort of load goes on there it drops to 0V. I put a 100K resistor on and it dropped right down, I'm just looking for what is expected so we can tune our factory's "pass/fail" criteria.
Mike
Oh, OK. Now, I understand. If you are letting it float, then yes, it will show whatever internal voltage PACK+ sees wrt PACK-. I thought you were asking me when the gauge is in system (with the load resistance) then if you turn the FETs off, what voltage you would see. The answer to that was 0.
But yes, you are right, if there is no load or connection between PACK+ and PACK-, it will internally float as you say.