Other Parts Discussed in Thread: TLV61046A, TPS61240
Hello!
We have TLV61046A EVM. I need help with the following: EVM does not make 5V output with the parameters mentioned in the subject and below.
Our circuit goal is the following:
Input: 3.0 - 4.2V
Output: 5.0V, 100mA (75mA nominal)
The EVM has the following changes:
R1 = 374k
L1 = VLCF4020T-100MR85
C2 = 10uF/10V + 22uF/25V, or only 10uF/10V
Input supply = workbench power supply
Load = resistors
Observations:
1) With 100mA load, EVM output is ~2.5V if TLV61046A is enabled while input voltage is < 3.9V*; switching period becomes 2.4us with 15% duty cycle (switch on)
1a) if the input voltage is lowered in 0.1V steps, the output remains 5V until input is < 2.1V
2) With 50mA load, output is ~2.5V if TLV61046A is enabled while input voltage is < 3.1V; switching period and duty cycle are similar to item 1 above.
2a) if the input voltage is lowered in 0.1V steps, the output remains 5V until input is < 1.6V
3) For the parameters stated in the above "circuit goal", WebBench reports "Duty Cycle is lower than the minimum for this device". If I lower input voltage to 3.8V, WebBench has no error.
* 3.9V becomes 3.7V if 10uF/10V cap is used without 22uF/25V present.
Any recommendations? larger inductor?
Side note: we like the output disconnect feature.
Many Thanks!
David McRell