This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

BQ25570: Cold start on BQ25570 EVM

Part Number: BQ25570

Hi Team,

   My customer is testing BQ25570 cold start based on TI EVM. They connect VIN to power supply source B2902(0.1v, current limit 1.5A). Then increase voltage in VIN with 10mv steps. But they only see VSTOR change when VIN come to 450mv, which is different from typical 330mv, max 400mv in the datasheet. 

  What might cause this problem, or the measurement method is not correct?