Other Parts Discussed in Thread: UCC28083
Team,
Can you please confirm the below:
-The datasheeet gives the min/max "start threshold voltage" page 3 of SLUS488E. Can it be assume that the VDD min/max specs are the same as the "start threshold voltage"?
If not could you provide the the VDD min/max?
-Please confirm that the UCC38083/UCC28083 does include a Zener diode on the VDD input.
-The VDD absolute max rating of the input are given at page 3 of SLUS488E (VDD 15V, Supply current 20mA).
Does it mean that this max value is the absolute limit the diode is specified for?
Bu what are the electrical characteristic (in normal operation, not the absolute limit) for which the diode is designed for?
Thanks in advance,
Anthony