This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

Discharging the battery with the Bq25703A module

Other Parts Discussed in Thread: BQ25703A

Hi,

I am using bq25703A for the battery Charger. I manage to establish a communication between this module and the card STM32F4 .
The communication is well established and I manage to write and read data in the registers of bq25703A also I manage to charge a battery that consists of 3 cells now I try to unload the same battery.
I followed the activation steps of the OTG and I finally succeeded, but my initial problem was the discharge of the battery.

When I activate the OTG the discharge will be done directly or it is necessary to add a charge.

If yes, how can I add the charge? in the datasheet there is a part that says "The device supports USB OTG operation to deliver power from the battery to other portable devices through USB port "but where is the USB port I do not see?

Regards,

Mohamed