Other Parts Discussed in Thread: TPS54360, , TPS2372, TPS2373, TPS23880, , UCC2897A, PMP20859
hi sir/madam,
Now I have made a router case, using POE power supply (TPS2378+TPS54360), the power is greater than 30W. Now I use two TPS2378+TPS54360 to power the system. Now the following situation appears:
1. When I use the switch to supply power to the router, first I plug in one portPOE&PSE.pdf and the power is normal. When I plug in RJ45 to supply power to another port, the system will lose power, and the power will be recharged at a interval of 2 seconds
2. This will not happen when I use two switches to supply power to two ports. When the two switches were connected together, there was a situation like 1.
Attached is the schematic diagram, please help to see if there is any change to improve this situation, thank you ~~~