This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

TPS50601-SP: Test of the Boot-PH and Error Amp per the spec.

Part Number: TPS50601-SP

When measuring the source/sink current of the error amplifier through the comp pin do I force 1V into the comp pin then remove it so I can force current into and out of this pin? When I do this the polarity of the current on the comp pin changes which makes since. Is this correct? Do I need to raise and lower the voltage on the sense pin as well? Just concerned about stressing the device.