Hi,
I would like to care for in-rush current when I use LM5060.
LM5060 has Fault delay function using with timer pin.
- During delay period, will the device have limit for output current and voltage?
- Or is the function only for delay period not to detect fault condition?
- If user would like to care for in-rush current, he should add external cap at output as attached file?
Regards,
Nagata.