This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

My customer is looking for TI altanative device of ONSEMI, NCP4304.

Part Number: UCC24612
Other Parts Discussed in Thread: UCC24610,

Hello guys,

 One of our customers is looking for TI altanative device of  ONSEMI, NCP4304.

 www.onsemi.com/.../NCP4304-D.PDF

 I think UCC24610 and UCC24612 could be used instead of NCP4304. Also I think UCC24612 is better than UCC24610 because UCC24612 deice is optimized more than UCC24610.

 Which device is beter to replace NCP4304? Or if TI have any other device to replace NCP4304, could you please let me know?

 Your reply would be much appreciated.

 Best regards,

 Kazuya Nakai.

  • Hello Kazuya,

    For a DCM, QR and ACF flyback and LLC the UCC24612 is the most compatible driver we have to the NCP4304 gate driver we have. The UCC24612 has 1 A of source driving capability and 4 A of sink capability.

    It uses a special gate drive technique that allows SR FETs to be driven at frequencies up to 1 MHz. This is describe in section 7.3.2 in detail in the data sheet.

    Regards,

    Mike
  • Hello Mike,

    Thank you for your reply. I will propose UCC24612 to the customer.

    Best regards,
    Kazuya Nakai.