Other Parts Discussed in Thread: BQ78350-R1
Dear
According to the be76930 data sheet (section 7.3.1.1.3 16-Bit CC), it write the following statements
The following equation shows how to convert the 16-bit CC reading into an analog voltage if no board-
level calibration is performed:
CC Reading (in µV) = [16-bit 2’s Complement Value] × (8.44 µV/LSB)
What does "no boarding level calibration is performed" mean?
Do i need to do calibration for current? i don't find any cue about doing current adc calibration in data sheet
Thanks