Part Number: BQ40Z60
Other Parts Discussed in Thread: BQSTUDIO
Hello,
I'm currently setting protections parameters using the bq40z60. I have some questions related to the thresholds.
1) Regarding CUV, which value should I put, compared to the cut-off discharge voltage given by the battery's datasheet? 10% more?
2)Regarding COV, which value should I put for safety? Would 90% of the maximum charging voltage be fine?
3) I have the same kind of questions for overcurrent in charge and discharge.
In short, are there usual values compared to the cells' datasheet values to use as protection thresholds?
Thank you.
Regards,
Marie