Hi team,
I have a question about TPS7B63-Q1.
Customer wants to use TPS7B63-Q1 as standard watchdog mode. Is TPS7B63-Q1 standard watchdog mode when WTS is connected OUT(5V) pin?
Regarding to pin FMEA consideration, customer hopes to avoid short condition between VBAT and GND condition.
In case of WTS has failure mode which is short to next pin which is GND pin, there is possiblity to happen VBAT-GND short condition if WTS is connected VBAT. So, customer don't want to connect WTS to VBAT, but they hope to connect WTS to OUT. Can WTS be connected OUT pin if TPS7B63Q1 set as standard watchdog mode?
Regards,
Nishimura