Hello,
a customer of mine wants to use the internal diodes next to the darlington array of the ULN2003A to conduct the discharge current of an external capacitor.
Attached to the ULN2003A is a RC filter (100R, 100nF ceramic) which will be switched to GND by the ULN2003A. This filter is filtering a PWM signal of 20kHz.
Can the internal diodes be used to conduct the discharging current of the capacitor or is an external diode needed? Can a diode with an high forward voltage be used or is a shottky diode needed?
Thank you!