This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

LP5018: 1. PWM frequency? 2. Use of single colour LEDs

Part Number: LP5018


Hello all,

my customer needs a PWM frequency of min. 3kHz. Is this possible with our LP5018, or has the customer use the 29kHz?

My customer has in his application 7  RGB-LEDs, but in addition 6 single colour LEDs. How should my customer connect the single colour LEDS.

Best regards

Egon

  • Hi, Egon,

    LP5018 has fixed PWM frequency of 29kHz, which is out of audio nosie range.

    Actually every channel can drive the single color LED except when you consider Bank function.

    Let me know if you have more questions.

    Thanks.

    Regards,

    Kenneth