This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

TPS23861EVM-612: TPS23861EVM-612 module PSE output is not working

Part Number: TPS23861EVM-612
Other Parts Discussed in Thread: LM5019

We Designed PD device and powering of using TPS23861EVM-612 module (POE +) .Last week is working fine.Today we are trying to power up the device using TPS23861EVM-612 module is not working .

We measured input voltage of TPS23861EVM-612 is ok and measured another supply (3.3V) it is under the limit.

We are connecting the ethernet cable in port j20 to PD device. 

We are trying to capture the power up sequence is not happening. PD device Ethernet voltage is zero.

Requested give some solution