Part Number: LM5022
Tool/software: WEBENCH® Design Tools
I want to get a Bode plot simulation under different load conditions. I'm designing a boost supply with 24V input and 100V/0.5A output. Webench runs the Bode plot with 200 ohm load - that's correct for 0.5A. But when I go to change to a lighter load, I get the input shown below which gives a min/max of 5/100 - it won't even let me put in the default value of 200. What's going on?