Section 2.3 of the bq78PL114 Tech Ref. says that a EUV condition clears when all cells go above the "hardware recovery level". But, there is a EUV Recovery setting for the '114 that, according to the Tech Ref, is normally set to 2700mV.
Is the "hardware recovery level" the same as the "Minimum startup voltage" of 2.9V from the datasheet? If so, why is a value of 2700mV recommended for the EUV Recovery setting?
Thanks!