Hi,
We are using the BQ24105 charger chip. The charger is set up for single cell charging and current limited to 500mA charging. On connecting a battery or dc source the charge led Stat1 comes on. However when the battery volts is a 4.09v and charge current has dropped the charge led STAT1 flashes and never indicates fully charged STAT2 on. Using a dc source if I set the voltage to 4.1v the charged led STAT2 turns on.
The datasheet only mentions 104,108 and 109 as having blinking status pins. What is the 105 indicating? Is it one of the faults listed for the blinking status pins?
Thanks
Carl