Part Number: TLV810
In the attached schematic,
- TLV810S is U54
- I'm trying to provide a reset (Active High, >100msec) to U15
- I would like to have two options to provide a reset
- TLV810S for hardware reset
- RESET_S is controlled by a micro processor, which can provide a software-based reset.
The software reset, RESET_S, currently works but I would prefer to have the TLV810S to provide the reset so it is ready on power-on.
Could you review to see if the circuit can provide the reset from both options?
Regards,
Andrew