Hi
In the bq76930 datasheet, it shows the belowing sentences at page38.
If the SCD delay setting is not setting 400us, for example 70us, what will happen for SCD?
Does the SCD protection early occur at 166mV when the SCD threshold setting is 200mV?
"Short circuit in discharge delay setting. A 400-μs setting is recommended only in systems using
maximum cell measurement input resistance, Rc, of 1 kΩ (which corresponds to minimum internal cell
balancing current or external cell balancing configuration)."