This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

ISO5452: Soft Turn-Off with Increased Drive Current

Part Number: ISO5452


Hello Team,

Please help with our customer's question about ISO5452:

In datasheet page 33 there are Figure 57(Current Buffer for Increased Drive Current):
Will Soft Turn-Off (STO) function work with it? 
How will it work with Increased Drive Current? When will it turn on?

Thank you in advance!

BR,
Ilya. 

  • Hi Ilya,

    A capacitor can be added to the base terminal of the BJT buffer. The capacitance can be sized based on the soft turn-off timing. In case of the DESAT detection, the driver pull-down current is 130mA.

    With Regards,

    Xiong

  • Hello Xiong,

    Thank you for the reply!

    If 10nF capacitance is added it provides huge increase in on/off delay during operation. (to 500-1000 ns).
    This leads to an increase of switching loss in IGBT.

    If they add capacitance lower than 10 nF, then it leads to the too much tempo of soft turn-off.
    Which leads to overvoltage on IGBT in case of short-circuit breaking current.

    Is there another way to apply soft turn-off in this scheme?

    Thank you in advance!

    BR,
    Ilya.
  • Hi Ilya,

    We can reduce the gate resistance value between driver output and base of BJT buffer to reduce the delay. 

    With Regards,

    Xiong