Hi Sir,
My customer is using LM5122 as boost structure and one of board is burned. There is several question need to be checked
spec : input 42~60V , Output 60V, 3A
1. Could LM5122 be use as non sync boost structure? From the result , the mos (SW to gnd ) is burned and diode is fine.
2. Boost Diode DBST : Is 1N4148 is ok for this and is possible the reason to induce LM5122 burn ?
3.If input cap and output cap is very small (around 1u) , is possible the reason to induce LM5122 burn ?