Hello,
I have a requirement for a new project to be able to keep itself alive for a short while in the event of an external power failure. At the moment I am using an encapsulated DCDC converter to provide 5V to the system. This 5V is then also used to deliver 3.3V via a LDO.
I'm fairly happy with the current DCDC converter, so I was wondering if a one-chip solution existed that would allow me to charge a battery from this regulated 5V supply, and maintain the 5V output using the battery as the source if that failed. The maximum current this would have to deliver is ~350mA.
In order to reduce the design time and deliver a reliable solution quickly I was hoping to find a highly integrated solution. Can anyone make a recommendation for a part that might fit my requirements here?