I’m working in the lab with a power supply prototype and I’m wondering if there are minimum pulse-width requirements for the UC2825A?
As I run the input voltage up on my supply, the duty cycle shrinks. I get to a certain pulse-width (~700ns) and the controller starts pulse-skipping. I’ve looked for a bad ramp, noise on the error-amplifier, or current-limit, but they all look clean.
I reduced the switching frequency from 187kHz to 140kHz and I was able to bring the input voltage up to a higher level before pulse-skipping began.
Any thoughts on this would be appreciated.